OTP refresh sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTP refresh sequence

935 Views
geekAbyo
Contributor I

Hi,

I am trying to understand what is the correct sequence to initiate an OTP refresh for PCA2131 product.

Based on the current datasheet, I understand that the sequence shall be like:

During a POR, set OTPR bit = 0, set OTPR bit = 1, wait 100ms (polling on value to see if it was set to 1), break out of the polling in case OTPR bit was set to 1.

Can someone explain if this is correct?
Thanks.

Best regards.

Tags (2)
0 Kudos
Reply
1 Reply

911 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Abyo,

your process is correct, however please make sure the oscillator is stable before you start the OTP refresh. Please check on the CLKOUT pin if the oscillator is stable before you start the OTP refresh process. 

JozefKozon_0-1757933839590.png

Also please note, that the VDD>1.8V and the rising speed must be minimally 2V/100ms. 

JozefKozon_1-1757933947439.pngJozefKozon_2-1757933976366.png

With Best Regards,

Jozef