Not able to Enter in sleep mode properly if wakeup source is Active low GPIO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not able to Enter in sleep mode properly if wakeup source is Active low GPIO

897 次查看
pratikyadav
Contributor II

Hello @Kan_Li

I am using PN7462 (EVK). I want to wake up my board from sleep mode.

I am using the following code to enter into sleep mode. After Executing the following API board is not responding.

 

 

 

 

void test_sleep()
{
//RfLd detection settings
phhalPcr_RfLdtParams_t sRfLdParams ={0, 0, 0, 0};


//Wake up sources selection GPIO is selected as wakeup source
phhalPcr_WakeUpConfig_t WakeUpConfigs= {0,0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 1, 0};



//Standby prevention reason
phhalPcr_StandbyPrevReason_t sStandbyPrevReason = 0;

uint32_t pwrDownConfig = E_APPLY_ALL_SETTNGS & ~(E_PD_GPIO2 ) ;
phhalPcr_Init( (phhalPcr_PwrTempConfig_t *)gpkphCfg_EE_Boot_PcrPwrTempConfig,
(phhalPcr_TxAnaStandByConfig_t *)gpkphCfg_EE_Boot_TxAnaStandByConfig,
pwrDownConfig);


//As phhalPcr_Init clear wakeup configuration init GPIO2 in input
phhalPcr_ConfigInput(2, true, true, true, true, false, false);

//Pullup GPIO2
phhalPcr_ConfigPuPd(2,true,false);


//Powerdown VDDOUT
phhalPmu_PvddLdoStop(); //TODO : Due to this BON setup wakes up without motion.
phhalPmu_PvddLdoLowPower();
DEBUG_PRINTF("\n Goint into sleep mode! \n");

//Enter into low power mode
phhalPcr_EnterLowPowerMode(&sRfLdParams, &WakeUpConfigs, &sStandbyPrevReason);
}

 

 

 

 

 

If I configure GPIO2 as a active high I am able board is going into sleep and wakeup on rising edge on GPIO2. 

 

 

 

 

//As phhalPcr_Init clear wakeup configuration init GPIO2 in input
phhalPcr_ConfigInput(2, true, true, true, false, false, false);

//PullDown GPIO2
phhalPcr_ConfigPuPd(2,false,true);

 

 

 

 

Can you please let me know if I have misconfigured or remaining to configure?

0 项奖励
回复
1 回复

850 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @pratikyadav ,

 

I am sorry, but seems only a transition from 0 to 1 can be used as a wake up event, please kindly refer to the following for details.

PN7462 GPIO wake up.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复