Noise Figure Tuning Network

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Noise Figure Tuning Network

1,832件の閲覧回数
spflanze
Contributor I

In spec sheets such as this one:

https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fdata-sheet%... 

there is are smith charts showing noise figure versus reflection coefficient data. In these smith charts does the reflection coefficient plotted in them show what it would without the transistor connected and the tuning network alone, or does it show what it is with the transistor connected?

In other words, to calculate what component values the tuning network had to have for any given reflection coefficient does the transistor base terminal's hybrid pi parameters have to be taken into account?

In that spec sheet's Tables 8 and 9 on page 7, and Table 10 on page 8 there is an Rn/50 column. What is Rn?

0 件の賞賛
返信
1 返信

1,721件の閲覧回数
LPP
NXP Employee
NXP Employee

A noise circle is a locus of source impedances for a given noise figure as a function of frequency. Gamma values are provided as source reflection coefficient at 50 Ohm characteristic impedance. These are parameters of the signals source alone (without transistor connected).

>What is Rn?

Datasheet provides noise figure at the optimal source resistance. Rn is a fictitious equivalent noise resistance that is a measure of additional noise when the source resistance is not equal to the optimal value. Please, refer to the following documents:

https://ww2.minicircuits.com/app/AN60-040.pdf //equation #4
http://www.engineering-electronics.com/html/smith_chart_course.html //Matching example #13
http://www.ece.ucsb.edu/~long/ece145a/LNAdesign.pdf


Have a great day,
Pavel
NXP TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信