Need clarification about QSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need clarification about QSPI

Jump to solution
1,787 Views
manid
Contributor I

Capture.JPGwe are not used NAND and NOR flash, we are using QSPI and eMMC flash in LS1043A processor. NOR and NAND flash is mandatory for LS1043A??

if not mandatory ,how to configure the IFC pin?? like AD1 to A25,CLE, AVD etc.....

consider the above image. it is our current design. is it is ok????

0 Kudos
Reply
1 Solution
1,775 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> NOR and NAND flash is mandatory for LS1043A?

Not mandatory.

> how to configure the IFC pin?? like AD1 to A25,CLE, AVD etc..

Please refer to the AN5012 - QorIQ LS1043A Design Checklist, Table 10. IFC pin termination checklist.

View solution in original post

0 Kudos
Reply
1 Reply
1,776 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> NOR and NAND flash is mandatory for LS1043A?

Not mandatory.

> how to configure the IFC pin?? like AD1 to A25,CLE, AVD etc..

Please refer to the AN5012 - QorIQ LS1043A Design Checklist, Table 10. IFC pin termination checklist.

0 Kudos
Reply