Need Help for Linux Kernel support - SC16IS762 - provide any documentation to do this

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need Help for Linux Kernel support - SC16IS762 - provide any documentation to do this

1,728 次查看
mohanmts
Contributor I

am trying to use SC16IS762 with high transfer speed spi - is there any way to make it work

0 项奖励
回复
3 回复数

1,706 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Mohanasundaram,

Therefore, based on your last response, you are within the SPI dynamic parameters. The SC16IS762 device supports SPI clock speeds up to 15 Mbit/s.

In this case, could you please share a detailed description of your issue? Are you able to interface with the device?

 

You may find a SC16IS750_Linux driver attached. I do recommend to use it as a reference for your design.

Regards,

David

0 项奖励
回复

1,720 次查看
mohanmts
Contributor I

Yes these are well within the range. Am using 3.3v params.

0 项奖励
回复

1,723 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Mohanasundaram,

I hope all is great with you.

What is the SPI data rate used in your application? Are you within the parameters mentioned below?

diazmarin09_0-1661807309930.png

 

Regards,

David

0 项奖励
回复