NXP UDA1334A Adafruit-I2Sdecoder for 24bit resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP UDA1334A Adafruit-I2Sdecoder for 24bit resolution

1,560 Views
SujataLMtech
Contributor I

I am interfacing the Adafruit board for NXP-UDA1334A to a Bluetooth audio module, I can hear the clear audio output for 16bit resolution. 

When I try to configure the module for 24 bit resolution, I get noisy output. My Bluetooth module is master and I am using left-justified, nobit delay, I2S output from master. 

I have correctly selected the SF0-SF1 lines both high. 

I have tried to use re-sample frequency at master configuration as 44100 and 48000, but both gives same noise level.

I tried to use De-Emph to High but this also does not help much.

Is there any other setting I need to use for 24 bit operation?

I am only interfacing, BCLK, WSEL and DIN pins from adafruit board, the PLL pin grounded memaning hte chip is in audio mode.

 

Any suggestions?

Thanks in advance.

0 Kudos
Reply
1 Reply

1,538 Views
guoweisun
NXP TechSupport
NXP TechSupport

This IC had already EOL and no more related documentations supporting are available now.

0 Kudos
Reply