I am interfacing the Adafruit board for NXP-UDA1334A to a Bluetooth audio module, I can hear the clear audio output for 16bit resolution.
When I try to configure the module for 24 bit resolution, I get noisy output. My Bluetooth module is master and I am using left-justified, nobit delay, I2S output from master.
I have correctly selected the SF0-SF1 lines both high.
I have tried to use re-sample frequency at master configuration as 44100 and 48000, but both gives same noise level.
I tried to use De-Emph to High but this also does not help much.
Is there any other setting I need to use for 24 bit operation?
I am only interfacing, BCLK, WSEL and DIN pins from adafruit board, the PLL pin grounded memaning hte chip is in audio mode.
Any suggestions?
Thanks in advance.
This IC had already EOL and no more related documentations supporting are available now.