NXP NX3P1108UK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP NX3P1108UK

1,408件の閲覧回数
jasonteoh
Contributor I

Hi Sir/Mdm,

I was looking at the NXP NX3P1108UK Logic controlled high-side power switch.

and i had some question as below.

 

I didn’t see any restriction about if EN voltage can be higher than Vin voltage or not.

There are two conditions in my current design.

  1. Vin=1.2V, EN=2.5V
  2. Vin=1.2V, EN=3.3V

Could you please help to check if above condition are workable for this IC?

And tell me if there’s any restriction related to Vin and EN pin which is not clarified in spec.

Thank you.

0 件の賞賛
返信
1 返信

1,377件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jason,

There will be no problems as long as the following conditions are met:

Table 5.JPG

Table 8a.JPG

Table 8b.JPG

Best regards,

Tomas

0 件の賞賛
返信