NXP NX3P1108UK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP NX3P1108UK

1,407 Views
jasonteoh
Contributor I

Hi Sir/Mdm,

I was looking at the NXP NX3P1108UK Logic controlled high-side power switch.

and i had some question as below.

 

I didn’t see any restriction about if EN voltage can be higher than Vin voltage or not.

There are two conditions in my current design.

  1. Vin=1.2V, EN=2.5V
  2. Vin=1.2V, EN=3.3V

Could you please help to check if above condition are workable for this IC?

And tell me if there’s any restriction related to Vin and EN pin which is not clarified in spec.

Thank you.

0 Kudos
Reply
1 Reply

1,376 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jason,

There will be no problems as long as the following conditions are met:

Table 5.JPG

Table 8a.JPG

Table 8b.JPG

Best regards,

Tomas

0 Kudos
Reply