NXP LX2160A Booting Option using SSD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP LX2160A Booting Option using SSD

1,339件の閲覧回数
Aathi1122000
Contributor I

Does the  LX2160A NXP processor supports to  boot  the image from the SSD(NVMe).

If yes, Can anyone help on this

0 件の賞賛
返信
2 返答(返信)

1,225件の閲覧回数
Aathi1122000
Contributor I

I have three sources in my design to boot the LX2160A

000- Hard-Coded

001- SD card

010- EMMC

111- XSPI NOR

I have fixed my source by using the DIP switch as NOR by selecting 111. If the NOR image got crashes means, LX2610A has the control to scan the RCW move to the next source like  either SD card

 

Aathi1122000_0-1722602567771.pngAathi1122000_0-1722602567771.png

 

0 件の賞賛
返信

1,299件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

LX2160A doesn't support booting atf/u-boot from SSD, it supports booting Linux Kernel and rootfs filesystem from SSD.

0 件の賞賛
返信