NXP ICODE SLI (ISO 15693)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP ICODE SLI (ISO 15693)

4,220 Views
jldias59
Contributor I

Hello,

i started working with ICODE SLI, SLIX and SLIX2.

What i need is a board that help me to understand and develop this tags only ICODE

THAMKS

0 Kudos
Reply
3 Replies

4,002 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Jorge,

Please look at the next development board SLRC610: High-performance frontend for ICODE® products. I think this will be very useful for your application.

Regards,

Mario

0 Kudos
Reply

4,002 Views
jldias59
Contributor I

Hello Mario,

IS This development board Kit: CLEV6630A board for SLRC610 and MFRC630 NFC

Reader?

*Or: *PN5180 development board?

THANKS

Em ter, 2 de abr de 2019 às 14:37, mario_castaneda <[email protected]>

escreveu:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: NXP ICODE SLI (ISO 15693)

reply from Mario Ignacio Castaneda Lopez

<https://community.nxp.com/people/mario_castaneda?et=watches.email.thread>

in Other NXP Solutions - View the full discussion

<https://community.nxp.com/message/1133801?commentID=1133801&et=watches.email.thread#comment-1133801>

0 Kudos
Reply

4,002 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Jorge,

Yes, Please look at the development board link.

CLEV6630A: MFRC630 and SLRC610 NFC Frontend Development Board

Regards,

Mario

0 Kudos
Reply