NXP AFE- MC33771C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,531件の閲覧回数
prabhus
Contributor II

Hi  we were previously used TI BQ Series AFE,in that AFE during cell balancing need to consider Adjacent cell balancing or not. what ABOUT NXP AFE.Any cell any time  we can enable cell balancing ? or we need to consider some procedure for cell balancing algo

0 件の賞賛
返信
1 解決策
1,522件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Prabu,

The MC33771x allows balancing all cells at the same time with a current up to 300 mA without exceeding the max. junction temperature of 150C.

BR, Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,523件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Prabu,

The MC33771x allows balancing all cells at the same time with a current up to 300 mA without exceeding the max. junction temperature of 150C.

BR, Tomas

0 件の賞賛
返信