Dear YYT,
Thank you for your reply. I have a few more questions. When initializing my STM32H723ZGT6, the voltage is 3.3V, but the voltage on the VCCA side is 1.8V. Can I directly connect and use it? I am using UHS-1. Is the voltage on the VCCB side 3.3V during initialization, and switches to 1.8V after initialization is complete?
[A] No. This will destroy the NVT4858. Please refer to the Table 8. in the NVT4858 datasheet. You must make sure, that any of the values listed there are not exceeded. If the VCCA=1.8V and you will apply 3.3V to the I/O pins on the VCCA side, this will exceed the maximum limit (VCCA+0.3V=1.8V+0.3V=2.1V) and destroy the NVT4858.

With Best Regards,
Jozef