NTS0102

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTS0102

2,593 Views
niteshsahay
Contributor III

Hi

I am planning to use NTS0102 for I2C application.

Is this IC suitable.If suitable, do i need to put external pull up and what value can be used for I2C lines.

Regards

Nitesh

0 Kudos
Reply
3 Replies

2,421 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Nitesh,

I would recommend using dedicated I2C voltage level translators.

Best regards,

Tomas

2,421 Views
niteshsahay
Contributor III

Hi Thomas

Thanks for the confirmation.

Can you please suggest me any I2C based Level translator part number which qualifies for Automotive grade (-40 to 105).

I could not see in the attached link.

Regards

Nitesh

0 Kudos
Reply

2,421 Views
niteshsahay
Contributor III

Hi Tomas

In general why we cannot use NTS0102 for I2C based application.

Regards

Nitesh

0 Kudos
Reply