NTS0102

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTS0102

2,609件の閲覧回数
niteshsahay
Contributor III

Hi

I am planning to use NTS0102 for I2C application.

Is this IC suitable.If suitable, do i need to put external pull up and what value can be used for I2C lines.

Regards

Nitesh

0 件の賞賛
返信
3 返答(返信)

2,437件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Nitesh,

I would recommend using dedicated I2C voltage level translators.

Best regards,

Tomas

2,437件の閲覧回数
niteshsahay
Contributor III

Hi Thomas

Thanks for the confirmation.

Can you please suggest me any I2C based Level translator part number which qualifies for Automotive grade (-40 to 105).

I could not see in the attached link.

Regards

Nitesh

0 件の賞賛
返信

2,437件の閲覧回数
niteshsahay
Contributor III

Hi Tomas

In general why we cannot use NTS0102 for I2C based application.

Regards

Nitesh

0 件の賞賛
返信