NAND Asynchronous Timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Asynchronous Timing

ソリューションへジャンプ
1,628件の閲覧回数
Daniel_M
Contributor I

I can't find tREA and tRHOH on the t4240 Reference Manual. I need these parameters to calculate the other tRCP min. 

Daniel_M_0-1630342656093.png

Daniel_M_1-1630342723135.png

 

 

 

 

 

タグ(1)
0 件の賞賛
返信
1 解決策
1,622件の閲覧回数
Bulat
NXP Employee
NXP Employee

tREA and tRHOH are parameters of the NAND flash devices, not T4240 ones. On the processor side we recommend to set correct data sampling point: IFC_FTIM2_CSn_NAND[TRAD]. It should be programmed as mention in section 12.5.7.3 of the Ref Manual:
"Read data sampling time (TRAD) represents the read data sampling time on the NAND. The value should be programmed where the sampling at the IFC should be done at the center of the received data eye. Its value can be calculated as [tREAmax (from NAND datasheet) + 2 x board delay + 1/2 received data window size]", where the 'receive data window size' is calculated as tRP - tREA + tRHOH.

Regards,

Bulat

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,623件の閲覧回数
Bulat
NXP Employee
NXP Employee

tREA and tRHOH are parameters of the NAND flash devices, not T4240 ones. On the processor side we recommend to set correct data sampling point: IFC_FTIM2_CSn_NAND[TRAD]. It should be programmed as mention in section 12.5.7.3 of the Ref Manual:
"Read data sampling time (TRAD) represents the read data sampling time on the NAND. The value should be programmed where the sampling at the IFC should be done at the center of the received data eye. Its value can be calculated as [tREAmax (from NAND datasheet) + 2 x board delay + 1/2 received data window size]", where the 'receive data window size' is calculated as tRP - tREA + tRHOH.

Regards,

Bulat

 

0 件の賞賛
返信