MW7IC915NT1 device input and output impedance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MW7IC915NT1 device input and output impedance

787件の閲覧回数
raveendrareddy
Contributor II

Hi Team,

I am planning to use MW7IC915NT1 device in one of my design and planning to operate in 1025 - 1150 MHz to replace obsolete MHVIC915R2 device.

I didn't find input and output impedance information form datasheet in the band of 1025 - 1150 MHz, would you please share the impedance details of the same.

Also I tried to simulate the model in AWR and I'm able to do simulate to certain level and would like to EM simulation, but I found that model is not linked with EM structure (no device cell attached to AWR model), would you please provide correct AWR model with device cell (footprint)

Regards,

Raveendra.

ラベル(1)
  • RF

タグ(1)
0 件の賞賛
返信
0 返答(返信)