Maximum rating of iput power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum rating of iput power

952 Views
chris_zhang
Contributor II

Hi,

Please help to advise the maximum ratings of input power for AFT27S010N, please help advise the spec., thanks.

Labels (1)
  • RF

0 Kudos
Reply
1 Reply

907 Views
LPP
NXP Employee
NXP Employee

We do not specify maximum input power for LDMOS devices since it depends on the amplifier design.

What is really important is the maximum gate-to-source voltage VGS = [-6.0,+10] V. Device would fail if this rating is violated. This limit can be reached in switch or class C amplifier modes.

In common linear amplifier modes, maximum VGS rating corresponds to very high input power (~40dBm). In practice, maximum input power is determined by a level that brings amplifier into strong saturation and may cause amplifier output to be overloaded. (If the drain power is switched off then VGS rating plays the rule.)

For example, AFT27S010N @ 2.14GHz in class AB mode, P3dB=42dBm, Gain=18.5dB -> Pin3dB=23.5dB. At this power level, the signal magnitude is 0.83V at DC bias 2.2V. It is far from the absolute maximum ratings for VGS.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply