MSDI Inputs as Outputs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSDI Inputs as Outputs

Jump to solution
2,030 Views
mark512
Contributor I

This is regarding the Multi Switch Detector Interface ICs.

On the datasheets for the MC33972, MC33975, MC34972 and MC34975, it's shown how the input wetting current supplies can be used like outputs to drive a small load like an LED.

On the datasheets for the MC33978, MC34978, CD1020 and CD1030, this application is not mentioned, but at a first glance it seems that there is no reason why these ICs wouldn't be able to do this as well. Is someone able to confirm that this works on these ICs too?

Thanks in advance!

0 Kudos
Reply
1 Solution
2,017 Views
guoweisun
NXP TechSupport
NXP TechSupport

No problem for them( MC33978, MC34978, CD1020 and CD1030) to drive LED. 

View solution in original post

0 Kudos
Reply
1 Reply
2,018 Views
guoweisun
NXP TechSupport
NXP TechSupport

No problem for them( MC33978, MC34978, CD1020 and CD1030) to drive LED. 

0 Kudos
Reply