MPC8347 in PCI host mode, acting as a PCI target

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8347 in PCI host mode, acting as a PCI target

2,726 次查看
admin
Specialist II
Does anybody know if it is possible to have the MPC8347 configured to be in PCI host mode and a PCI device acting as an initiator writing some data to the MPC8347 memory?
If it's possible, do I only have to set inbound address translation to do that?

We have an MPC8347 in host mode driving an FPGA on the PCI bus. The MPC8347 must be able to configure the FPGA by setting registers located in BAR0 of the FPGA (MPC8347 being the initiator in this case). Once the FPGA is configured we want to request the FPGA to push data to the MPC8347 memory (the FPGA being the initiator in this case).

Any clarification will help,

Best regards
0 项奖励
回复
2 回复数

1,402 次查看
oded_asulin
Contributor I
which PCI are you using PCI1 or 2?
0 项奖励
回复

1,402 次查看
admin
Specialist II
The MPC8347 has only one PCI interface which corresponds to the PCI1 interface of the MPC8349.
0 项奖励
回复