MPC8347 in PCI host mode, acting as a PCI target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8347 in PCI host mode, acting as a PCI target

2,727 Views
admin
Specialist II
Does anybody know if it is possible to have the MPC8347 configured to be in PCI host mode and a PCI device acting as an initiator writing some data to the MPC8347 memory?
If it's possible, do I only have to set inbound address translation to do that?

We have an MPC8347 in host mode driving an FPGA on the PCI bus. The MPC8347 must be able to configure the FPGA by setting registers located in BAR0 of the FPGA (MPC8347 being the initiator in this case). Once the FPGA is configured we want to request the FPGA to push data to the MPC8347 memory (the FPGA being the initiator in this case).

Any clarification will help,

Best regards
0 Kudos
Reply
2 Replies

1,403 Views
oded_asulin
Contributor I
which PCI are you using PCI1 or 2?
0 Kudos
Reply

1,403 Views
admin
Specialist II
The MPC8347 has only one PCI interface which corresponds to the PCI1 interface of the MPC8349.
0 Kudos
Reply