MPC5777C Development Board/Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C Development Board/Kit

Jump to solution
2,041 Views
berat24
Contributor III

Hello everyone,

I would like to ask a question about MPC5777C development board.

When I examined MPC5777CEVBUG.pdf document, I saw that BOOTCFG pins have been connected to PC1 and PC6 pads respectively. However, I could not understand which pads have been connected to eSCI_0 RX and TX pins on development board.

Could you help me?

Btw, there is a photo below from my development board.

Sincerely.

 

0 Kudos
Reply
1 Solution
2,003 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

I can't see problem here - the USB-UART bridge should work with Rappid. It's standard converter which should be recognized as UART port in Rappid bootloader.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
3 Replies
2,024 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

RXDA and TXDA pins of eSCI_0 (GPIO 89 and 90) are connected only to USB/UART transceiver FT232RQ. These signals are not available on pin headers.

If you want to have these signals on pin headers, use other GPIOs, there are more routing options. See System IO Definition xls file for details.

Regards,

Lukas

0 Kudos
Reply
2,005 Views
berat24
Contributor III

Hi,

I understood that I cannot use BAM module(serial bootloader) on development board because it does not have eSCI_0 Rx ve Tx connections to pads. Am I wrong?

Sincerely.

 

0 Kudos
Reply
2,004 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

I can't see problem here - the USB-UART bridge should work with Rappid. It's standard converter which should be recognized as UART port in Rappid bootloader.

Regards,

Lukas

0 Kudos
Reply