MPC5744P Master code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P Master code

45,840件の閲覧回数
padmalathagudip
Contributor I

Iam working on MPC5744p Controller. I am trying to implement the SPI Master driver code for same controller, for this i selected DSPI0(SPI0) and implemented SPI in this way as shown in " MPC5744_SPI_master docx." after flasing i connected to CRO to check ransfered data with the pin  MISO but Master is not showing anything from MPC5744P board when i transmitted 'A'.  SO please help me on this. Tell me is there any mistakes in this code and need to modify anything.? Can you please send the code for SPI Master . Tell me if any links are there .  after this iam trying to transfer from MPC5744P(Master ) to AVR(Slave) controller but garbage value is coming on UART.

Regards,

Padmalatha

ラベル(1)
0 件の賞賛
返信
0 返答(返信)