MPC5643L: Writing User Option Status: Disable Watchdog

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5643L: Writing User Option Status: Disable Watchdog

ソリューションへジャンプ
2,909件の閲覧回数
bastian_schick
Contributor IV

Hi,

 

I want to disable the watchdog (and switch to DP mode). But I see no way to write UOS register.

Also mine is all ones. Is this correct for  a brand new chip ?

0 件の賞賛
返信
1 解決策
2,307件の閲覧回数
gernot
Contributor I

you have to write a line in shadow flash using debugging tools.

 

in this website look for application note AN4034:

 

title: MPC5643L Dual Processor Mode

 

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,307件の閲覧回数
dayve
NXP Employee
NXP Employee

Hey!

 

What debug tools are you using? I am working on some information that might be of use to you.

 

Regards, 

Dayve

0 件の賞賛
返信
2,307件の閲覧回数
Tatay
Contributor II

Hi,

 

I'm usiin CW 2.7 for MPC5643L with debugger PE micro USB multilink. I don't manage to switch to DPM whereas there is an option to create a project in DPM. But this doesn't put the MCU in DPM.

how should i do to switch to DPM? The macro "mpc5643L_enable_second_core_vle.mac" doesn't work, most of instructions finish with invalid command!

 

Thank you,

 

Best regards

0 件の賞賛
返信
2,308件の閲覧回数
gernot
Contributor I

you have to write a line in shadow flash using debugging tools.

 

in this website look for application note AN4034:

 

title: MPC5643L Dual Processor Mode

 

 

 

 

0 件の賞賛
返信