MPC5643L: Writing User Option Status: Disable Watchdog

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5643L: Writing User Option Status: Disable Watchdog

跳至解决方案
2,898 次查看
bastian_schick
Contributor IV

Hi,

 

I want to disable the watchdog (and switch to DP mode). But I see no way to write UOS register.

Also mine is all ones. Is this correct for  a brand new chip ?

0 项奖励
回复
1 解答
2,296 次查看
gernot
Contributor I

you have to write a line in shadow flash using debugging tools.

 

in this website look for application note AN4034:

 

title: MPC5643L Dual Processor Mode

 

 

 

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,296 次查看
dayve
NXP Employee
NXP Employee

Hey!

 

What debug tools are you using? I am working on some information that might be of use to you.

 

Regards, 

Dayve

0 项奖励
回复
2,296 次查看
Tatay
Contributor II

Hi,

 

I'm usiin CW 2.7 for MPC5643L with debugger PE micro USB multilink. I don't manage to switch to DPM whereas there is an option to create a project in DPM. But this doesn't put the MCU in DPM.

how should i do to switch to DPM? The macro "mpc5643L_enable_second_core_vle.mac" doesn't work, most of instructions finish with invalid command!

 

Thank you,

 

Best regards

0 项奖励
回复
2,297 次查看
gernot
Contributor I

you have to write a line in shadow flash using debugging tools.

 

in this website look for application note AN4034:

 

title: MPC5643L Dual Processor Mode

 

 

 

 

0 项奖励
回复