Hi,
During my experiments with the MPC5554EVB development board, I successfully initialized the external RAM (starting a 0x20000000).
But now I would like to force the linker to place some variables in this external memory and to keep the other ones in the SRAM.
I tried to create new sections in my lcf file:
MEMORY{ pseudo_rom: org = 0x40000000, len = 0x00009000 init: org = 0x40009000, len = 0x00001000 exception_handlers: org = 0x4000A000, len = 0x00001000 internal_ram: org = 0x4000B000, len = 0x00002000 heap : org = 0x4000D000, len = 0x00001000 stack : org = 0x4000E000, len = 0x00001000 external_ram: org = 0x20000000, len = 0x00080000}SECTIONS{...GROUP : { .ext_ram_text (TEXT) : {} .ext_ram_data (DATA) : {} } > external_ram}
and in my code I declare the variable that I want to place in external RAM like this:
#pragma section data_type ".ext_ram_data" __declspec(section ".ext_ram_data") uint8_t buffer[512];
But I'm getting compilation errors...
Error : sections used for data must have an uninitialized data sectionError : unknown section name '.ext_ram_data'
Thanks in advance for your help,
Olivier
解決済! 解決策の投稿を見る。
Hello
Can you try to modify the variable definition as follows:
#pragma section data_type ".ext_ram_data" ".ext_ram_data" __declspec(section ".ext_ram_data") uint8_t buffer[512];
The variable buffer is not initialized. So you need to specify a uname section in the pragma section.
See Power Architecture Build Tools Reference.pdfm chapter Pragmas for Power Architecture Compiler section Library and Linking Pragmas > section.
CrasyCat
i'm new to the 5554 but i suspect the line that reads
.ext_ram_data (DATA) : {}
needs to have information insides the braces.
this is toolset-dependet stuff, to some extent, i think.
tell us what you are using
Hello
Can you try to modify the variable definition as follows:
#pragma section data_type ".ext_ram_data" ".ext_ram_data" __declspec(section ".ext_ram_data") uint8_t buffer[512];
The variable buffer is not initialized. So you need to specify a uname section in the pragma section.
See Power Architecture Build Tools Reference.pdfm chapter Pragmas for Power Architecture Compiler section Library and Linking Pragmas > section.
CrasyCat
Hi i have tried using the below statements, compiler gives error
#pragma section TRYme ".tryme" ".tryme" __declspec(section ".tryme") extern char OS_TrapHndl_TrapAddr;
the variable OS_TrapHndl_TrapAddr is declared in other source file.
i am using it in MPC5674,
The compiler error is " error (dcc:1633): parse error near '".tryme"'"
can some one pls say if there are any settings needed for the __declspec to be made.
Thanks in advance.
Regards,
Sumanth
Hello
Two issues here:
1- The __declspec should be specified in a new line (not on the same line as the pragma.
Apparently Lithium did remove the line breaks in my original code snippet.
2- The declspec should be done on both the variable definition and declaration,
CrasyCat
Hello CrasyCat,
Thanks for the reply.
i have changed as follows in one file apart from the source file where OS_TrapHndl_TrapAddr; is declared(static UINT32 OS_TrapHndl_TrapAddr
xyz.c
#pragma section TRYme ".tryme" ".tryme"
__declspec(section ".tryme") extern UINT32OS_TrapHndl_TrapAddr;
the compiler issues the error message "error (dcc:1633): parse error near '".tryme"'" refers to (section ".tryme")
i am trying to move the variables declared in other source files to a new section(without touching the source code). my approach is correct or is there any other way of doing it.
Thanks & Regards,
Sumanth
Hello
First parameter in pragma section identifies the type of object stored in the section.
TRYMe is not a valid object type.
Did you try:
#pragma section data_type".tryme" ".tryme"
__declspec(section ".tryme") extern UINT32OS_TrapHndl_TrapAddr;
CrasyCat
Hello ,
i have also tried the statements u sent. the error still occurs at 2 line that is " __declspec(section ".tryme") extern UINT32OS_TrapHndl_TrapAddr"
error is : parse error near '".tryme"'
i am not using code warrior, i am using Tasking EDE with wind river DIab compiler 5.8.0.0
the user manual for the diab compiler doesnot contain the __declspec, pls confirm whether the __declspec would work in this environment.
pls also confirm that without modifying the .c file, if it would be possible to move variables to new section.
Hello
The notation __declspec(section ".tryme") extern UINT32OS_TrapHndl_TrapAddr is only working with CodeWarrior compilers.
If you are using another compiler, please check with the compiler provider how you can define variables in a user defined section.
CrasyCat
Hello,
Thanks a lot for your response!
Now the variable "buffer" is correctly placed in the external RAM.
Olivier