MPC5200 large flash boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5200 large flash boot

2,310 Views
jima
Contributor I
I just upgraded my board from 16Mbyte-8bit FLASH to 64Mbyte-16bit FLASH (S29GL512N).  I can not get it to boot, has anyone else tried booting from this size flash?

My boot jumpers are set to: non-mux, 16bit data, no swap, Max wait, 0x100 boot exception, Large_fl selected, most_graphics not selected.

My config changed as follows:
BOOTSTR:  from-FF00 to-FC00
CSBOOTCR: from-00047800  to-00047D00

The interesting thing is that with the CodeWarrior USB-TAP I can burn and verify the flash.  But when I try to execute, or inspect flash I get garbage.

The biggest question is:  Has anyone booted in LARGE FLASH mode?

Thanks in advance for your reply.

0 Kudos
Reply
1 Reply

1,512 Views
JonKeeble
Contributor I
We are having problems with the same jumper settings.
 
Did this ever get resolved?
 
We use uboot and get as far as booting linux 2.6 (tftp)  but after downloading the kernel and running linux the network is unusable
 
jon
0 Kudos
Reply