MPC5125 - IEEE 1588 sync capability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5125 - IEEE 1588 sync capability

ソリューションへジャンプ
2,077件の閲覧回数
Champaka
Contributor III

Hi all,

         could anyone tell me if MPC5125 processor has IEEE 1588 (Precision Time Protocol) sync capability ??

タグ(1)
0 件の賞賛
返信
1 解決策
1,843件の閲覧回数
TomE
Specialist II

http://www.freescale.com/webapp/sps/site/application.jsp?code=APLIEEE_1588

 

The MCP5125 isn't listed on the above page.

 

"Freescale began shipping processors with hardware timestamp capabilities in 2007."

 

The MCP2515 is in the right time frame, but doesn't seem to have hardware support for IEEE 1558.

 

It depends on how accurate you need the timestamp. If you don't need the accuracy of the hardware timestamping then software timestamps might be an option.

 

Tom

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,844件の閲覧回数
TomE
Specialist II

http://www.freescale.com/webapp/sps/site/application.jsp?code=APLIEEE_1588

 

The MCP5125 isn't listed on the above page.

 

"Freescale began shipping processors with hardware timestamp capabilities in 2007."

 

The MCP2515 is in the right time frame, but doesn't seem to have hardware support for IEEE 1558.

 

It depends on how accurate you need the timestamp. If you don't need the accuracy of the hardware timestamping then software timestamps might be an option.

 

Tom

 

0 件の賞賛
返信
1,843件の閲覧回数
Champaka
Contributor III

   k....    thank you  :smileyhappy:

0 件の賞賛
返信