MPC5125 - IEEE 1588 sync capability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5125 - IEEE 1588 sync capability

Jump to solution
966 Views
Champaka
Contributor III

Hi all,

         could anyone tell me if MPC5125 processor has IEEE 1588 (Precision Time Protocol) sync capability ??

Tags (1)
0 Kudos
Reply
1 Solution
732 Views
TomE
Specialist II

http://www.freescale.com/webapp/sps/site/application.jsp?code=APLIEEE_1588

 

The MCP5125 isn't listed on the above page.

 

"Freescale began shipping processors with hardware timestamp capabilities in 2007."

 

The MCP2515 is in the right time frame, but doesn't seem to have hardware support for IEEE 1558.

 

It depends on how accurate you need the timestamp. If you don't need the accuracy of the hardware timestamping then software timestamps might be an option.

 

Tom

 

View solution in original post

0 Kudos
Reply
2 Replies
733 Views
TomE
Specialist II

http://www.freescale.com/webapp/sps/site/application.jsp?code=APLIEEE_1588

 

The MCP5125 isn't listed on the above page.

 

"Freescale began shipping processors with hardware timestamp capabilities in 2007."

 

The MCP2515 is in the right time frame, but doesn't seem to have hardware support for IEEE 1558.

 

It depends on how accurate you need the timestamp. If you don't need the accuracy of the hardware timestamping then software timestamps might be an option.

 

Tom

 

0 Kudos
Reply
732 Views
Champaka
Contributor III

   k....    thank you  :smileyhappy:

0 Kudos
Reply