MPC5121 Linux BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5121 Linux BSP

2,984 Views
martinw
Contributor III

Hi,

 

Probably a silly question, but here goes:

 

I want to lift some drivers from the Linux bsp for the ADS5121.  I have installed Debian Linux, applied the Freescale BSP and run LTIB.

 

So far I haven't been able to find the sources for the drivers - speicifically it's the DIU I'm interested in.

 

Can anyone guide me to finding the driver sources under the Linux installation please?

 

Cheers


Martin

0 Kudos
Reply
1 Reply

1,344 Views
medina
Contributor III

Hello,

 

I don't understand  your question entirely but I will try to answer:

 

- If you want the kernel sources from your host, you need to install the appropriate package from your distribution and kernel that install the sources under /usr/src.

- If you want the kernel sources from ltib, you can see the packages under /opt/freescale/pkgs/. Also you can "install" the sources (with patches): "./ltib -p kernel -m scprep" , you can see the sources under ltib/rpm/BUILD/linux.

- If you want a specific driver you can find it under the folder drivers.

 

I hope it will help

 

Regards,

Medina

0 Kudos
Reply