MPC-LS-VNP-RDB 100Base-T1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC-LS-VNP-RDB 100Base-T1

939件の閲覧回数
babay1996
Contributor I

Hello, I want to realize network communication on the MPC-LS-VNP-RDB reference board. After I get the new reference board, I rewrote the system and set the system to start from EMMC. By configoring the network port IP, the network port of RJ45 on the board (Eth1,Eth4,Eth5,Eth6) can all communicate.The configuration is shown below, but the on-board Ethernet does not communicate.In general, eth1-1g can also connect to SJA1105, it can communicate, which means that the configuration of SJA1105 is good, but 100BASE-T1 can not communicate, I don't know why?

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)