MPC 5644A serial boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC 5644A serial boot

ソリューションへジャンプ
2,110件の閲覧回数
stanleyli
Contributor II

Hello all,

I am developing serial boot for MPC 5644a.

The thing is that i can not read echo from mpc 5644a when i gave a echo command (id= 0x01 with 8 bytes password).

The EVB I am using is xPC56xx EVB which is xPC564AADPT with XPC56xx EVB motherboard.

The jump J7 for boot mode set to serial mode already, but the CAN message always shows error frame.

Is there any setting i need to consider?

TKS

タグ(1)
0 件の賞賛
返信
1 解決策
1,870件の閲覧回数
stanleyli
Contributor II

I figure it out by myself.

I have to consider the status of EVTO pin which is to determine what baud rate mode you choose.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,871件の閲覧回数
stanleyli
Contributor II

I figure it out by myself.

I have to consider the status of EVTO pin which is to determine what baud rate mode you choose.

0 件の賞賛
返信
1,870件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Other Freescale Solutions ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 件の賞賛
返信