MPC 5644A serial boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC 5644A serial boot

跳至解决方案
2,111 次查看
stanleyli
Contributor II

Hello all,

I am developing serial boot for MPC 5644a.

The thing is that i can not read echo from mpc 5644a when i gave a echo command (id= 0x01 with 8 bytes password).

The EVB I am using is xPC56xx EVB which is xPC564AADPT with XPC56xx EVB motherboard.

The jump J7 for boot mode set to serial mode already, but the CAN message always shows error frame.

Is there any setting i need to consider?

TKS

标记 (1)
0 项奖励
回复
1 解答
1,871 次查看
stanleyli
Contributor II

I figure it out by myself.

I have to consider the status of EVTO pin which is to determine what baud rate mode you choose.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,872 次查看
stanleyli
Contributor II

I figure it out by myself.

I have to consider the status of EVTO pin which is to determine what baud rate mode you choose.

0 项奖励
回复
1,871 次查看
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Other Freescale Solutions ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 项奖励
回复