MOB10 Digital Signature

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MOB10 Digital Signature

3,114 次查看
trantuananh
Contributor I

Hi, can this product perform ECDSA. Brs

0 项奖励
回复
8 回复数

3,025 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @trantuananh ,

 

MOB10 is a packaging type not of product.

We currently offer JCOP4 and JCOP4.5 in this package type, both of which support ECDSA.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,020 次查看
trantuananh
Contributor I
Tk u for your reply. Does JCOP4.5 support EDDSA
0 项奖励
回复

3,015 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @trantuananh ,

 

Yes, it supports!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,010 次查看
trantuananh
Contributor I

Hi,

Can I order same samples of JCOP 4.5 from you? If yes, please send me link to order and ship to Vietnam

Kind Regards

0 项奖励
回复

3,005 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @trantuananh ,

 

I am sorry, but this is just a tech support channel. For commercial topic, please kindly contact your local Disti for further help. You may refer to https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS for more details.

 

Thanks for your patience and understanding!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 项奖励
回复

2,995 次查看
trantuananh
Contributor I

I would like to ask two more questions regarding technical support

- I am using JCshell tool for customizing JCOP4. Can I use the same tool for JCOP4.5.

- Is the SCP03 script used for JCOP4 the same as one used for JCOP4.5

Brs

0 项奖励
回复

2,986 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @trantuananh ,

 

Yes , you can, and handling of SCP03 is the same.

 

however, I would recommend using the later version that comes with JCOP4.5 tools.

This version has some features which are enabled uniquely for JCOP4.5 which you may find useful.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,022 次查看
trantuananh
Contributor I

Hi Kan

Tk u for your reply. Does JCOP4.5 support EDDSA

Brs

0 项奖励
回复