MMZ09332BT1 technical problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMZ09332BT1 technical problem

1,953 次查看
liuxialsp
Contributor I

1. Is pin 10 POWERDOWN control 1.8V control? Control BIAS power only? Normal work is to ground PDC (Bias "On"), then why is the current 0mA in the following table? VCC1,VCC2 Do we also need external control power supply on and off?

2. Are pins 4 and 5 suspended or grounded? Schematic diagram is suspended, PCB diagram is grounded

3. How to connect pins 7, 8 and 9? The schematic diagram is connected together, pin 7 of PCB diagram is VCC2 input, pin 8 and 9 are RF output

0.png1.png2.png

标签 (1)
  • RF

标记 (1)
0 项奖励
回复
1 回复

1,938 次查看
LPP
NXP Employee
NXP Employee

1.
Datasheet Table 3 provides Power Down Current as the current through the PDC pin. PDC uses negative logic and should be grounded if not used (capacitor can be removed). On/Off Voltage levels are provided. VCC1 and VCC2 consumption in the power down mode is low but it is not specified. There is no need for external control of VCC1/VCC2 supplies.

2.
Pins 4 and 5 are not internally connected. They can be left open or grounded.

3.
These leads are connected by wire bonds to the common pad on the die. So, they are electrically tied together. However, each wire bond introduces some inductance. On the evaluation board, one pin is used for DC bias to separate RF path from DC bias. Doing that may increase VBW of the circuit. It is not mandatory to separate connections. Though, i suggest to follow reference design.