MFS5600AMBA0ES in-line program interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFS5600AMBA0ES in-line program interface

2,708件の閲覧回数
EMertCakir
Contributor III

Hello 

I will use MFS5600AMBA0ES and MC33PF8200DEES in a project. MC33PF8200DEES has an in-line program interface as shown below. But I have not come across such an interface for MFS5600AMBA0ES. Which pins should I use to program MFS5600AMBA0ES permanently?

WhatsApp Image 2023-12-12 at 01.03.13.jpegWhatsApp Image 2023-12-12 at 01.03.13.jpeg

 

 

ラベル(3)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,677件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

This document is under NDA, do you have access to Secure Files?

Please go to Automotive Dual Buck Regulator and Controller with Voltage Monitors and Watchdog Timer FS5600, sign in, go to Documentation and click on Secure Files.

If you have access you will find the application note there, if not, please request access.

 

 

0 件の賞賛
返信

2,694件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Please refer to application note AN13263 OTP programming instructions for FS5600.

Best regards.

2,686件の閲覧回数
EMertCakir
Contributor III

Hello 

Link is broken

Page Not Found

 

0 件の賞賛
返信