MFR4310 designed question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFR4310 designed question

2,630 Views
xudb
Contributor II

Hi everybody:

    We want to designed a product about flexray bus communication, and we want to chose the mfr4310 for the main controller and the  mcu MPC5125 for config the mfr4310, but there is a question : we need two cold startup nodes, does the mfr4310 can config two keyslot,or not? should we use two mfr4310?OR there have some soc whitch contain 2 flexray channels??Hope someone can provide suggestions!! THANKS!!!!

THE MFR4310 datasheet about feature describe: "Internal channel A and FlexRay Port A can be configured to be connected to physical FlexRay channel A or physical FlexRay channel B " ,is it means we can config two keyslot? one is connected to Internal channel A  and the other is connected to FlexRay Port A? we just want one node be a auxiliary node to wakeup and syn the bus.

0 Kudos
Reply
6 Replies

1,224 Views
juunna
Contributor I

I am currently using two MC9S12XF512 chips configured as coldstart nodes to wake up an MFR4310 for FlexRay communication. All other parameters are configured identically, following the same protocol, FlexRay 2.1. Why can't they wake up the MFR4310? Can they communicate successfully? Are there any incompatibilities?

I want the official website routine of Freescale's MFR4310 chip to implement FlexRay communication. Where can I find it?

0 Kudos
Reply

2,607 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @xudb 

MFR4310 is in End Of Life status, it is not available anymore. So, we do not support new designs.I recommend to select a microcontroller with in-built Flexray module.

Regards,

Lukas

0 Kudos
Reply

1,223 Views
juunna
Contributor I

DEAR sir :Good afternoon! I am currently using two MC9S12XF512 chips configured as coldstart nodes to wake up an MFR4310 for FlexRay communication. All other parameters are configured identically, following the same protocol, FlexRay 2.1. Why can't they wake up the MFR4310? Can they communicate successfully? Are there any incompatibilities?

I want the official website routine of Freescale's MFR4310 chip to implement FlexRay communication. Where can I find it?

0 Kudos
Reply

2,597 Views
xudb
Contributor II

Hi lukaszadrapa:

     Currently, Our product is base on MPC560xP series, and it just have a flexray port A to connect to the channel A or B, and have a key slot config only, How CAN I config it to have two key slot ??

    By the way , have any suggustion for mcu selection?

0 Kudos
Reply

2,591 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Take a look at https://community.nxp.com/t5/MPC5xxx/Two-keyslot-setting/m-p/852425

An option is MPC57xx family or devices like S32G, S32R or preproduction S32E and S32Z. But based on provided information, MPC57xx should be better option, mentioned S32 devices have unnecessary features.

Regards,

Lukas

0 Kudos
Reply

2,584 Views
xudb
Contributor II

Hi  lukaszadrapa:

       Thanks very nuch for your reply,  Another question is  does the MPC5125YVN400 1M01S QAX1604Al has any flexray module ? I havnt found any msg in the datasheet ,I am not sure anyone on the family series mcu have not flexray module, Or ,someone of the series mcu include flexray module?

      What is the diffence of flexray v3.0 and v2.1 ? And Is flexray v3.0 compatible with v2.1?We can designed the board base v3.0 ,and communication with the v2.1 nodes?

0 Kudos
Reply