MC34845 current capability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC34845 current capability

1,765 次查看
hcontigiani
Contributor II

Hi,

    I am looking at the MC34845 datasheet and I was wondering why it can only handle total of 180mA (30mA per channel) when it has a 2.1A Boost switch?

    His brother MC34844 has a 2.5A boost switch and it is able to manipulate 80mA per channel. It is true that MC34845 can only manipulate backlight of 180mA?

    Thanks, Hernán.

标记 (2)
0 项奖励
回复
1 回复

1,700 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Thank you for writing.

Unfortunately, it is true that the MC34845 can only handle a total of 180 mA.

The main difference between his brother, is because the MC34844 can drive 10 outputs. That is why the MC34844 has higher boost output.

I hope this answers your question.

Best regards,

Diego.

0 项奖励
回复