MC34844 Current Mirror Error Reduction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC34844 Current Mirror Error Reduction

1,928件の閲覧回数
elizabeth_lee
Contributor I

I'm trying to drive 4 strings of LEDs at near-constant current using the MC34844. Is it possible to improve the current mirror error on the MC34844 from the +/-2% on the datasheet?

For instance, connecting 2 channels to each string of LEDs to 'average out' the error? Or adding peripheral current sense feedback?

Or are there any recommendations on driving 4 strings of LEDs, near-constant current, adjustable from 0-30mA?

Thanks!

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,907件の閲覧回数
elizabeth_lee
Contributor I

Thanks for the reply! Is there no external circuitry I can design to reduce the error?

0 件の賞賛
返信

1,907件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Please get note that the current error accuracy is fixed inside of IC,you can't modify!

0 件の賞賛
返信