MC34844 Current Mirror Error Reduction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC34844 Current Mirror Error Reduction

1,925 Views
elizabeth_lee
Contributor I

I'm trying to drive 4 strings of LEDs at near-constant current using the MC34844. Is it possible to improve the current mirror error on the MC34844 from the +/-2% on the datasheet?

For instance, connecting 2 channels to each string of LEDs to 'average out' the error? Or adding peripheral current sense feedback?

Or are there any recommendations on driving 4 strings of LEDs, near-constant current, adjustable from 0-30mA?

Thanks!

Tags (1)
0 Kudos
Reply
2 Replies

1,904 Views
elizabeth_lee
Contributor I

Thanks for the reply! Is there no external circuitry I can design to reduce the error?

0 Kudos
Reply

1,904 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Please get note that the current error accuracy is fixed inside of IC,you can't modify!

0 Kudos
Reply