MC33664 conected to MC33771 or MCU by SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC33664 conected to MC33771 or MCU by SPI

跳至解决方案
1,012 次查看
wenfengyao
Contributor II

wenfengyao_0-1655458636647.jpeg

Regarding the above picture, I have the following questions
1. Why are SPI_TX and SCLK_TX the same line?
2. Should there be SPI_RX not shown in this diagram?
3. If I connect two MC33664, does SPI DATA need two wires or can I use the same wire?

0 项奖励
回复
1 解答
1,006 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jacky,

the Figure 38. in the MC33771C datasheet is incorrect. For the connection of the loop-back daisy chain please refer to the Figure 2. in the UM11334. Please also refer to this link. You might find it useful.

With Best Regards,

Jozef

在原帖中查看解决方案

0 项奖励
回复
2 回复数
979 次查看
wenfengyao
Contributor II

Thank you for your help

1,007 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jacky,

the Figure 38. in the MC33771C datasheet is incorrect. For the connection of the loop-back daisy chain please refer to the Figure 2. in the UM11334. Please also refer to this link. You might find it useful.

With Best Regards,

Jozef

0 项奖励
回复