MC33664 conected to MC33771 or MCU by SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33664 conected to MC33771 or MCU by SPI

Jump to solution
673 Views
wenfengyao
Contributor II

wenfengyao_0-1655458636647.jpeg

Regarding the above picture, I have the following questions
1. Why are SPI_TX and SCLK_TX the same line?
2. Should there be SPI_RX not shown in this diagram?
3. If I connect two MC33664, does SPI DATA need two wires or can I use the same wire?

0 Kudos
1 Solution
667 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jacky,

the Figure 38. in the MC33771C datasheet is incorrect. For the connection of the loop-back daisy chain please refer to the Figure 2. in the UM11334. Please also refer to this link. You might find it useful.

With Best Regards,

Jozef

View solution in original post

0 Kudos
2 Replies
640 Views
wenfengyao
Contributor II

Thank you for your help

668 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jacky,

the Figure 38. in the MC33771C datasheet is incorrect. For the connection of the loop-back daisy chain please refer to the Figure 2. in the UM11334. Please also refer to this link. You might find it useful.

With Best Regards,

Jozef

0 Kudos