Regarding the above picture, I have the following questions
1. Why are SPI_TX and SCLK_TX the same line?
2. Should there be SPI_RX not shown in this diagram?
3. If I connect two MC33664, does SPI DATA need two wires or can I use the same wire?
Solved! Go to Solution.
Thank you for your help