MC1322x GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC1322x GPIO

Jump to solution
2,099 Views
sar02
Contributor I

Hi there.

I am having huge problems trying to get some simple GPIO set up on the Low Power node from the ZigBee Development Kit.

I have tried using the software drivers defined in the documentation, tried to alter GPIO control registers directly via the documentation in the reference manual and finally tried to manually alter states of the registers by using pointers to the base memory addresses of the relevant registers.

With each attempt the outcome was no voltage on any of the GPIO pins on the Low Power Node which I am trying to set as an output HIGH.

Any example code or a run through of the correct procedure to initialise GPIO if anyone else has used these pins would be greatly appreciated.

Scott

Labels (1)
  • RF

Tags (3)
0 Kudos
Reply
1 Solution
1,770 Views
AlanCollins
Contributor V

Hello Scott.

        I recommend you to use the Demo applications as reference. For example: SMAC demo uses the GPIO driver to turn ON/OFF the LEDs in the evaluation boards. 

#define Led1Off()           (void)Gpio_SetPinData(LED1_PIN, LED_RESET)   /* Set      LED1 to OFF state */

You may init the GPIO by using the driver (option 1), or else writing direclty into the registers (option 2):

OPTION 1:

if (LEDNr & LED1){

    Gpio_SetPinFunction(LED1_PIN, gGpioNormalMode_c);  // LED1_PIN = gGpioPin23_c

    Gpio_SetPinReadSource(LED1_PIN, gGpioPinReadReg_c);

    Gpio_SetPinDir(LED1_PIN, gGpioDirOut_c);

  Gpio_SetPinData(LED1_PIN, gGpioPinStateHigh_c);

OPTION 2:

static void PlatformInitGpio(void)

{

  GPIO_REGS_P->DataLo = gDataLoValue_c;                  //MBAR_GPIO + 0x08

  GPIO_REGS_P->DataHi = gDataHiValue_c;                  //MBAR_GPIO + 0x0C

  GPIO_REGS_P->DirLo =  gDirLoValue_c;                   //MBAR_GPIO + 0x00

  GPIO_REGS_P->DirHi =  gDirHiValue_c;                   //MBAR_GPIO + 0x04

  GPIO_REGS_P->PuEnLo = gPuEnLoValue_c;                  //MBAR_GPIO + 0x10

  GPIO_REGS_P->PuEnHi = gPuEnHiValue_c;                  //MBAR_GPIO + 0x14

  GPIO_REGS_P->FuncSel0 = gFuncSel0Value_c;              //MBAR_GPIO + 0x18

  GPIO_REGS_P->FuncSel1 = gFuncSel1Value_c;              //MBAR_GPIO + 0x1C

  GPIO_REGS_P->FuncSel2 = gFuncSel2Value_c;              //MBAR_GPIO + 0x20

  GPIO_REGS_P->FuncSel3 = gFuncSel3Value_c;              //MBAR_GPIO + 0x24

  GPIO_REGS_P->InputDataSelLo = gInputDataSelLoValue_c;  //MBAR_GPIO + 0x28

  GPIO_REGS_P->InputDataSelHi = gInputDataSelHiValue_c;  //MBAR_GPIO + 0x2C

  GPIO_REGS_P->PuSelLo = gPuSelLoValue_c;                //MBAR_GPIO + 0x30

  GPIO_REGS_P->PuSelHi = gPuSelHiValue_c;                //MBAR_GPIO + 0x34

  GPIO_REGS_P->HystEnLo = gHystEnLoValue_c;              //MBAR_GPIO + 0x38

  GPIO_REGS_P->HystEnHi = gHystEnHiValue_c;              //MBAR_GPIO + 0x3C

  GPIO_REGS_P->PuKeepLo = gPuKeepLoValue_c;              //MBAR_GPIO + 0x40

  GPIO_REGS_P->PuKeepHi = gPuKeepHiValue_c;              //MBAR_GPIO + 0x44

}

I hope this helps.

View solution in original post

0 Kudos
Reply
1 Reply
1,771 Views
AlanCollins
Contributor V

Hello Scott.

        I recommend you to use the Demo applications as reference. For example: SMAC demo uses the GPIO driver to turn ON/OFF the LEDs in the evaluation boards. 

#define Led1Off()           (void)Gpio_SetPinData(LED1_PIN, LED_RESET)   /* Set      LED1 to OFF state */

You may init the GPIO by using the driver (option 1), or else writing direclty into the registers (option 2):

OPTION 1:

if (LEDNr & LED1){

    Gpio_SetPinFunction(LED1_PIN, gGpioNormalMode_c);  // LED1_PIN = gGpioPin23_c

    Gpio_SetPinReadSource(LED1_PIN, gGpioPinReadReg_c);

    Gpio_SetPinDir(LED1_PIN, gGpioDirOut_c);

  Gpio_SetPinData(LED1_PIN, gGpioPinStateHigh_c);

OPTION 2:

static void PlatformInitGpio(void)

{

  GPIO_REGS_P->DataLo = gDataLoValue_c;                  //MBAR_GPIO + 0x08

  GPIO_REGS_P->DataHi = gDataHiValue_c;                  //MBAR_GPIO + 0x0C

  GPIO_REGS_P->DirLo =  gDirLoValue_c;                   //MBAR_GPIO + 0x00

  GPIO_REGS_P->DirHi =  gDirHiValue_c;                   //MBAR_GPIO + 0x04

  GPIO_REGS_P->PuEnLo = gPuEnLoValue_c;                  //MBAR_GPIO + 0x10

  GPIO_REGS_P->PuEnHi = gPuEnHiValue_c;                  //MBAR_GPIO + 0x14

  GPIO_REGS_P->FuncSel0 = gFuncSel0Value_c;              //MBAR_GPIO + 0x18

  GPIO_REGS_P->FuncSel1 = gFuncSel1Value_c;              //MBAR_GPIO + 0x1C

  GPIO_REGS_P->FuncSel2 = gFuncSel2Value_c;              //MBAR_GPIO + 0x20

  GPIO_REGS_P->FuncSel3 = gFuncSel3Value_c;              //MBAR_GPIO + 0x24

  GPIO_REGS_P->InputDataSelLo = gInputDataSelLoValue_c;  //MBAR_GPIO + 0x28

  GPIO_REGS_P->InputDataSelHi = gInputDataSelHiValue_c;  //MBAR_GPIO + 0x2C

  GPIO_REGS_P->PuSelLo = gPuSelLoValue_c;                //MBAR_GPIO + 0x30

  GPIO_REGS_P->PuSelHi = gPuSelHiValue_c;                //MBAR_GPIO + 0x34

  GPIO_REGS_P->HystEnLo = gHystEnLoValue_c;              //MBAR_GPIO + 0x38

  GPIO_REGS_P->HystEnHi = gHystEnHiValue_c;              //MBAR_GPIO + 0x3C

  GPIO_REGS_P->PuKeepLo = gPuKeepLoValue_c;              //MBAR_GPIO + 0x40

  GPIO_REGS_P->PuKeepHi = gPuKeepHiValue_c;              //MBAR_GPIO + 0x44

}

I hope this helps.

0 Kudos
Reply