MC13224 Programming problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13224 Programming problem

1,807件の閲覧回数
KCZ
Contributor I

I can't program my own MC13224 PCBA no matter through JTAG or serial port, do anyone have this issue before? Please advise.  Thanks!

 

0 件の賞賛
返信
2 返答(返信)

1,354件の閲覧回数
lnl
Contributor I

Hi,

 

I'm having the same problem. I had the device soldered by professionals and none of 6 copies could be programmed. Have you found the problem?

 

0 件の賞賛
返信

1,354件の閲覧回数
redbee
Contributor III

Please contact me at [email protected]

 

I can probably help with the issue. A soldering problem is the most likely, although not if you've had it professionally done.

 

If you are confident that the soldering is good, then it could be a layout/hookup issue. 

 

Another common problem is that the part isn't erased (and therefore you can't enter the bootloader). This often happens when you flash it incorrectly. Try to do an hardware erase (with the VREF pins and reset). 

 

I can look over your schematic/hookup to find problems. I also have a variety of firmware tests that can help isolate the issue.

 

-Mar.

0 件の賞賛
返信