MAPBGA 121 Package Support PCB Mounting and Routing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MAPBGA 121 Package Support PCB Mounting and Routing

2,069件の閲覧回数
carlthomson
Contributor I

Hi. I'm designing a PCB with the MAPBGA 121 package. The package has 0.25mm - 0.35mm diameter balls on 0.65mm spacing. Even with a 0.25mm solder pad on the PCB, this ball pitch is too small to allow room for through-vias. I'm not finding any supporting documentation on land pattern recommendations, or routing strategies. Anyone have any experience with this package?

タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,524件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello Carl,

What is your Freescale device you working with? Would you provide Part Number?

Having this it will be easier to find info you asking for.

Regards,

Wlodek_D.

0 件の賞賛
返信

1,524件の閲覧回数
carlthomson
Contributor I

Wlodek,

Thank you for contacting me. The part in the design is the MK20DN512VMC10, which comes in the MAPBGA 121 package.

Thank you,

Carl

Date: Mon, 17 Mar 2014 07:53:03 -0700

From: [email protected]

To: [email protected]

Subject: Re: - MAPBGA 121 Package Support PCB Mounting and Routing

MAPBGA 121 Package Support PCB Mounting and Routing

reply from Wlodek_D. in Other Freescale Solutions - View the full discussion

Hello Carl,

What is your Freescale device you working with? Would you provide Part Number?

Having this it will be easier to find info you asking for.

Regards,

Wlodek_D.

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in Other Freescale Solutions by email or at Freescale Community

Following MAPBGA 121 Package Support PCB Mounting and Routing in these streams:

Inbox

0 件の賞賛
返信