Ltib and source control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ltib and source control

2,591件の閲覧回数
bandeg
Contributor I
Hello:
 
How do people generally add the LTIB to their own source control?   (CVS, Subversion)?
Should we treat the cross compiler, linux, and GPL and user packages differently?
 
How do you build the source from scratch on a new machine from your own source control.    Do you first just install the latest LTIB, then check out the latest from your source control?   Or is everything built from your source control?
 
Do you source-control the source for every package, or just check in the patches with the tarball, spec file updates, etc.
 
I suppose the binary files of packages that we never touch only need to be checked in as tarballs instead of source?
 
Your experience here would be appreciated so I don't have to learn things the hard way :smileywink:
 
B
 
 
 
0 件の賞賛
返信
2 返答(返信)

1,508件の閲覧回数
Nich
Contributor III

I have similar question... It is a pity that no one answered yet...

0 件の賞賛
返信

1,508件の閲覧回数
Nich
Contributor III

We have finally found a way to put LTIB under source control (SVN in our case).

 

While I was googling for that topic I have found a discusstion in LTIB mailing list, where it is said that "LTIB is intended more as a package publishing tool, not a software development tool so it should not be used for revision control" :smileyhappy:

 

But anyway we would like to have all our modifications in SVN :smileyhappy:

 

There were two problems for us:

  • Install LTIB on Ubuntu/Kubuntu 12.04
  • LTIB stores patches outside of directory where it is installed (by default /opt/freescale/pkgs)

 

First problem has been solved by my colleague with set of scripts, that he has found somewhere in the internet. These scripts don't solve all problems so he has added couple of his own scripts. Now it works fine for our BSP 20100413 for MPC8308ERDB and Ubuntu/Kubuntu 12.04. Zipped tarball with scripts is attached to this post and there is an original readme file inside.

 

Second problem has been solved in following way. I have added new parameter "our_patches" to ltib script. This is directory where I want to put all our patches. I have found a subroutine that implements "patchmerge" command and replaced lpp parameter with our_patches parameter. So now ltib put new patches in our-patches directory. Also I have added our-patches to ldirs definition. ldirs is a list of directories where ltib looks for the files. Also you need either to comment ldirs definition in .ltibrc file or to add our-patches there too.

 

    ldirs        => "$top/our-patches",    our_patches  => "$top/our-patches",

So now we can just pur all LTIB directory (after clean and without rootfs directory) under version control.

 

0 件の賞賛
返信