Mamba(5674F) development:Conversion of *.mot file to *.s19

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mamba(5674F) development:Conversion of *.mot file to *.s19

1,089件の閲覧回数
mra_cu
Contributor I

Hi,

I am developing the device drivers for Mamba(5674F). I am using Code warrior 2.10(CW55xx_v2_10_EVAL) version for my codebuild. The Codewarrior generates two files: 1. Executable file(*.elf) and the other is symbols file(*.mot). 

I would like to flash the files using Lauterbach T32 software. But T32 is looking for *.elf and *.s19 file.

 

1.Can any body help me in showing me how to convert *.mot to *.s19 file

2.or Can I flash *.elf and *.mot using the Lauter Bach T32 software

 

Rizwan

 

0 件の賞賛
返信
1 返信

592件の閲覧回数
TomE
Specialist II

You posted this question twice. Can you please delete the second copy?

 

Read the following:

 

http://en.wikipedia.org/wiki/SREC_%28file_format%29

 

"The Motorola S-record format is an ASCII hexadecimal ("hex") text encoding for binary data. It is also known as the SREC[1] or S19[2] format."

 

So I suspect the ".mot" file is the file you want. Just try changing its name.

 

Tom

 

0 件の賞賛
返信