Load Switch ILim Pin issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Load Switch ILim Pin issue

2,104件の閲覧回数
kiran1
Contributor I

Hi,

We are using the NX5P3290UKZ load switch in our design.
The input to the switch is 5V at 3A(max) and output is limited to 5V at 1A using resistor of 49.9Kohm on ILim pin of switch.
We are seeing an issue that when we power ON the board the ILim pin of switch get shorted with ground(0ohm with respect to ground).
Kindly let us know your thoughts on the same.

Thanks & Regards,

Kiran

0 件の賞賛
返信
3 返答(返信)

1,993件の閲覧回数
kiran1
Contributor I

Hi,

When we found that ILim pin got shorted with ground, we assumed load switch has gone bad and we replaced it with a new IC(Load switch). when we Powered it ON again we found a short on ILim pin. 

Please find the Load switch schematics below.

NXP_IMAGE.PNG

0 件の賞賛
返信

1,993件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

For your schematic please make sure:

1: C136 1nf/16V or 25V(at least).

2: Add external Schottky diode, NX5P3290 works well without it. To improve the lowest VBUS voltage during fast role swap, it is recommended to add a lower forward voltage diode, for example VF = 0.3 V.

3: Note the PCB layout, because of the CSP package with difficult solder. Suggest test the ILIM resistance with GND without power on.

0 件の賞賛
返信

1,993件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Could you please show us your schematic?

Can you make sure that this is not your solder issue?

0 件の賞賛
返信