Linker error 2019 Unresolved external Symbol _phBalReg_PcsWin_Init reference in Function _main

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linker error 2019 Unresolved external Symbol _phBalReg_PcsWin_Init reference in Function _main

1,281件の閲覧回数
sonnycagalingan
Contributor I

Hi Guys,

I am new here and I need help with the development of RD710 software I already compiled NxpRd.lib from the quick startup kit and included it to my solution using VS 2010 I am receiving Fatal Error LNK2019 Unresolved external Symbol  _phBalReg_PcsWin_Init reference in Function _main during building... I have already included the NxpRd.lib file as well as the header file in the project properties...any advise or tip is appreciated thanks...

0 件の賞賛
返信
0 返答(返信)